Open Connection Manager

Whether viewing or editing fiber connections, the procedure to open a fiber point feature in Connection Manager is the same.
  1. Click the Connection Manager button on the Fiber Manager toolbar.
  2. Use the Connection Manager  cursor to hover over a fiber feature until it highlights, then click it.

    TIP: If you select a feature that contains conflicts, the Connection Conflict Resolution tool opens.
  3. Connection Manager opens and displays the two fiber facilities that appear alphabetically first at that location.

QR code for this page

Was this helpful?