Using Circuit Manager

IMPORTANT: Geodatabase Manager is not supported with Fiber Manager Circuits. Do not use Geodatabase Manager to reconcile or post edits to Fiber Manager data if circuits are in use with the fiber data.

A circuit is a veritable path. You can create a circuit for a glass path without distinguishing the wavelengths that travel along that path. Or you can create a separate circuit for each wavelength on a glass path. Circuit Manager helps you:

  • Create and edit circuits associated with an end-to-end path in the fiber network

  • View and manage circuit information

  • Define and edit circuits along a connected path

  • Change the header (origin) of a circuit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.