DUG_IR Converter_CLP-01

Using IR key codes

If you do not know your television model number, you will need to discover the code set by operating a series of remote commands.
To add the device with series commands:
  1. On the Home page, tap All devices > IR Convertor.
  2. Tap on unused channel IR Convertor CH1 (A), (Unused channels have no name displayed against them).

    NOTE: IR Convertor channels CH6 to CH8 are only used with optional IR extension cable.

  3. Choose TV (B) as the device type then tap Continue.
  4. Select the television brand (C).

  5. Tap on the remote key (D) and check whether the television responds.
    NOTE: Confirm that the television is switched on and you can see the screen and network between the devices are unblocked.
  6. If the television shows the possible response tap on Does it work toggle switch (E).
  7. Tap on (F) for other remote key and repeat Step 5 and Step 6.
  8. Once the correct code set has been recognized, tap Continue (G).

  9. Tap on Confirm (H) on IR Config pop up.

    IR Convertor downloads the IR code set and the app displays the progress.
  10. Once download of IR code is complete, tap on Save.

On successful download, the television IR remote will be visible in the Wiser app Home page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?