DUG_IR Converter_CLP-01

Pairing the device

Using the Wiser app, pair your device with the Wiser Hub to access and control the device. You can either add the device manually or do an auto-scan to pair it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.