DUG_IR Converter_CLP-01

Using the Device

The Control Panel allows you to view the used and unused list of channels.

On the Home page, tap All devices > IR Convertor to access the control panel.

On the IR Convertor control panel page, you can see the following:

  • Battery level (A)

  • Broadcasting channel list (B)

  • Wired extension channel list (C)


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.