DUG_IR Converter_CLP-01

Troubleshooting

Symptom

Solution

The device is offline.

The battery may be low or drained. Replace the battery in the device.

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to resetting the device

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.