DUG_IPC_Outdoor_CLP-02

Configuring IR night vision

The infrared LEDs in the camera allows you to see and record a clear black and white video/image in the dark.
Follow the steps to configure the IR night vision:
  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap and tap Settings > IR night vision.
  3. Select any one of the following options:
    • Auto - Turns on/off automatically when the environmental light is below/above a certain threshold of the lux level
    • Off - Turns off the IR night vision at all times
    • On - Turns on the IR night vision at all times

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?