DUG_IPC_Outdoor_CLP-02

Removing the device

Using the Wiser app, you can remove a device from the device list.
Follow the steps to remove the device:
  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap icon and tap Settings.
  3. Tap Remove device (A) and tap Confirm.

    TIP: Alternatively, you can long tap on the IP Camera Outdoor on the home page to remove the device.
    NOTE:

    • Removing the device will reset the device. The LED starts blinking red indicating that the device is ready to pair with another network.

    • If there is a problem while pairing, refer to troubleshooting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?