Detection alarm setting
Follow the steps to enable the motion detection:
-
On the Home page, tap All devices > IP Camera Outdoor.
-
Tap the toggle switch (A) to turn On the Motion Detection Alerts.
Alarm sensitivity level
Using the Wiser app, you can adjust the sensitivity level of your motion detector.
Tap Alarm sensitivity level (B) and select any one of the following levels:
– Low
– Medium
– High
Activity area
Using the Wiser app. you can set the surveillance area for motion detection.
-
Tap the toggle switch (C) to enable the Activity area.
-
Tap Surveillance area settings (D) and drag/resize the red frame to set the surveillance area and tap Save.
-
The motion is detected only in the saved surveillance area.
-
The privacy zone detection area setting overrides the motion detection activity area setting. Therefore, even if the motion detection activity area is larger than the privacy zone detection area, the motion will only be detected within the privacy zone detection area.