DUG_IPC_Outdoor_CLP-02

Scheduling playback

Using the Wiser app, you can add a schedule that allows you to turn off/on recording automatically based on your needs.
Follow the steps to schedule the recording:
  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap and tap Settings > Recording Settings > Schedule.
  3. Tap Add schedule and set the time (A).
  4. Tap Repeat (B) and select the days you want the schedule to repeat.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule.
  7. Tap Local recording (E), select one of the options:
    • On - Turns on the recording during the scheduled time
    • Off - Turns off the recording during the scheduled time
    NOTE: The recording will be saved to the memory card.

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?