DUG_IPC_Outdoor_CLP-02

Using the device

Using the control panel of the IP Camera, you can see live video of the outdoors on the display screen and includes the following features:
Enables audio of the live video
Makes the video fullscreen
Takes screenshot of the live view
Lets you communicate with a person near the device
Records the live view
Enables motion detection
Enables private mode
View the stored images or videos
NOTE:
  • To view the notification/alarm messages, tap > Message.

  • To review the recordings using playback feature, refer to Playback.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?