8910CT9301R03/21

Factory Modifications

Factory Modifications

Modification

Form (add to the catalog number after the voltage code)

Factory installed auxiliary contacts

Contact your local Schneider Electric office.

Pressure wire connectors (30 A)

Y122

Box lugs (30 A)

Y239

DIN mounting bracket attached, 35mm
(available for 30–60 A devices only)

Y135

Type DP, 1 Pole 30–40 Full Load Amperes

Type DP, 2 Pole 30–40 Full Load Amperes

Type DPA, 2 and 3 Pole 30–40 Full Load Amperes

Type DPA, 4 Pole 30–40 Full Load Amperes

Type DPA, 2 and 3 Pole 50, 60, and 75 Full Load Amperes

Type DPA, 2 and 3 Pole 90 Full Load Amperes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.