990-5996D-001

Prepare the Battery Breaker Box for Cables

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or grommets with the gland plates installed, and do not drill or punch holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the gland plates:
    • For bottom cable entry: Remove the bottom gland plate.
    • For top cable entry – only available for the 60–80 kVA battery breaker box: Remove the top gland plate.

    E3MBBB60K80H

    E3MBBB60K80H

    E3MBBB100K200H

     
  2. Drill or punch holes for cables or grommets in the gland plate(s).
  3. Install grommets (if applicable) and refit the gland plate(s).
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.

    E3MBBB60K80H

    E3MBBB60K80H

    E3MBBB100K200H

     
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.