990-91274H-001

Final Installation

  1. Install the provided kick plates on the front, rear, and sides of the classic battery cabinet.
    NOTE: Only remove the kick plates when following the procedure for decommissioning or moving the classic battery cabinet. See Decommission or Move the Classic Battery Cabinet to a New Location for details.
  2. Close the door(s). On the 1000 mm wide classic battery cabinet, install two screws to close the left door.

    1000 mm Wide Classic Battery Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?