990-91274H-001

Optional Cable Kits for Line-Up Solutions

Two cable kits are available:

  • E3MOPT003: Cable kit that includes power cables and signal cables for installation of one classic battery cabinet adjacent to the 60–100 kVA UPS. This cable kit is for the 700 mm wide Easy UPS 3M Classic Battery Cabinet.

  • E3MOPT004: Cable kit that includes power cables and signal cables for installation of one classic battery cabinet adjacent to the 60–100 kVA UPS. This cable kit is for the 1000 mm wide Easy UPS 3M Classic Battery Cabinet.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.