990-91575-001

Final Installation

  1. Reinstall the four front covers.
    NOTE: Two different breaker covers are supplied with the empty battery cabinet. Install the breaker cover suitable for your battery breaker.

    Bottom Cable Entry System

    Top Cable Entry System

  2. Fasten the front anchoring bracket to the empty battery cabinet with M6 screws.

    Front View of Empty Battery Cabinet

  3. Mount the front anchoring bracket to the floor.
    NOTE: Floor anchoring bolts are not provided.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?