990-91575-001

Battery Requirements

Battery type VRLA
Minimum flammability rating HB
Battery shelves 4 shelves sized 1057 x 767 mm
Maximum weight per shelf 460 kg
Maximum weight per cabinet 1600 kg
Height between battery shelves 340 mm
Maximum battery height including battery terminals 240 mm
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?