990-91575-001

Position the Empty Battery Cabinet

DANGER
hazard of electric shock, explosion, or arc flash
Leave the empty battery cabinet covered while making anchoring holes to prevent dust or other conductive parts in the system.
Failure to follow these instructions will result in death or serious injury.
  1. Only for installation with two empty battery cabinets: Remove the indicated side panels from the battery cabinets on the adjacent sides.
  2. Position the empty battery cabinet(s) in the final installation area.
    NOTE: Leave 100 mm free space behind the empty battery cabinet(s) for airflow.
  3. Anchor the rear anchoring brackets to the floor.
    NOTE: Floor anchoring bolts are not provided.

    Rear View of the Empty Battery Cabinet

  4. Only for installation with two empty battery cabinets: Install the top baying brackets between the empty battery cabinets.

    Front View of Two Empty Battery Cabinets

  5. Remove the indicated four covers.

    Front View of the Empty Battery Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?