990-91202A-001

Environment

  Operation Storage
Temperature 0 °C to 40 °C (32 °F to 104 °F) -25 °C to 55 °C (-13 °F to 131 °F)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?