990-91202A-001

Trip Settings

  400 V Systems 208 V Systems
  10 kW 15 kW 20 kW 30 kW 40 kW 10 kW 15 kW 20 kW
Ir setting 112 112 112 112 144 112 112 144
Im setting 1250 1250
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?