990-5994B-001

Prepare the Parallel Maintenance Bypass Panel for Cables

DANGER
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the parallel maintenance bypass panel.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the top and bottom gland plates.

    Top of Parallel Maintenance Bypass Panel

    Bottom of Parallel Maintenance Bypass Panel

  2. Drill or punch holes for cables or grommets in the gland plates.
  3. Install grommets (if applicable) and refit the gland plates.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.

    Top of Parallel Maintenance Bypass Panel

    Bottom of Parallel Maintenance Bypass Panel

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.