990-5994B-001

Connect the Signal Cables for Easy UPS 3M

NOTE: Route the signal cables separately from the power cables.
  1. Remove the plastic cover of the maintenance bypass switch MBB to get access to the AUX switches.
  2. Connect signal cables (not supplied) from the three AUX switches in the maintenance bypass switch MBB to the UPSs.
  3. Fasten the signal cables to the cable reliefs.
  4. Close the inner door and fasten with screws.
  5. Close the front door.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.