990-5994B-001

Mount the Parallel Maintenance Bypass Panel to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the maintenance bypass panel to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware for the wall/rack type.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations and mount the anchor bolts.
  3. Remove the screws and open the inner door.
  4. Mount the parallel maintenance bypass panel to the wall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.