990-91078G-001

Connect the Power Cables in the 40 kVA 400 V / 20 kVA 208 V UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the conduit box cover.

    Rear View

  3. In dual mains systems, remove the three single mains brackets.
  4. Route the power cables through the conduit box.
  5. Connect the PE cable to the PE terminal.
  6. Connect the input, output, and bypass (if applicable) cables.
  7. Connect the battery cables.
  8. Reinstall the conduit box cover.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?