990-91078G-001

Input Contacts and Output Relays

Input Contacts

NOTE: When an external battery breaker with ON/OFF status detection and trip function is used, leave the terminator installed between J7–1 and J7–2.
NOTE: Schneider Electric recommends to connect the optional temperature sensor kit E3SOPT003 (R25=5 kohm, B25/50=3275) to J2 to monitor the battery temperature.
NOTICE
Risk of equipment damage
  • Connect the Schneider Electric shunt trip coil LV429390 to the recommended battery breaker to protect the battery.
  • The battery breaker contact drive (J6–1) can provide a maximum of +24 V, 200 mA to the shunt trip coil. If this value is exceeded it can damage the UPS.
Failure to follow these instructions can result in equipment damage.

Input connections are considered 24 VDC Class 2/SELV.

Input Contacts for UPSs without Batteries

Output Relays

Output relay connection: Maximum 3A/240 VAC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?