990-91078G-001

Appendix: Switch/Breaker Details

3:3 UPS

  Model Switch/Breaker Description Switch or Breaker
10 kVA

UIB

OSMC65H4C32

32A 4P

Breaker

SIB

OSMC65H4C32

32A 4P

Breaker

UOB

A9S68432 

32A 4P

Switch

MBB

OSMC65H3C32

32A 3P

Breaker

BB

A9S68332

32A 3P

Switch (for UPSs with internal batteries)

15 kVA

UIB

OSMC65H4C40

40A 4P

Breaker

 

SIB

OSMC65H4C40

40A 4P

Breaker

 

UOB

A9S68440

40A 4P

Switch

 

MBB

OSMC65H3C40

40A 3P

Breaker

 

BB

A9S68363 

63A 3P

Switch (for UPSs with internal batteries)

20 kVA

UIB

OSMC65H4C63

63A 4P

Breaker

 

SIB

OSMC65H4C63

63A 4P

Breaker

 

UOB

A9S68463 

63A 4P

Switch

 

MBB

OSMC65H3C50

50A 3P

Breaker

 

BB

A9S68363

63A 3P

Switch (for UPSs with internal batteries)

30 kVA

UIB

A9S68480

500VAC 80A 4P

Switch

 

SIB

A9S68480

500VAC 80A 4P

Switch

 

UOB

A9S68480

500VAV 80A 4P

Switch

 

MBB

A9S68363

500VAC 63A 3P

Switch

 

BB

A9S68391

100A 3P

Switch (for UPSs with internal batteries)

40 kVA

UIB

A9S68492

125A 4P

Switch

 

SIB

A9S68492

125A 4P

Switch

 

UOB

A9S68492

125A 4P

Switch

 

MBB

A9S68380

80A 3P

Switch

 

BB

A9S68392 

125A 3P

Switch (for UPSs with internal batteries)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?