990-91078G-001

Communication Interfaces

10-15 kVA 400 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

20-30 kVA 400 V / 10-15 kVA 208 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

40 kVA 400 V / 20 kVA 208 V UPS

  1. Dry contacts

  2. Parallel ports

  3. USB (for service)

  4. RS485

  5. RS232 (for service)

  6. Network management card (NMC)

  7. Cold start (optional)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?