990-66239-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.
NOTE: The recommended rear clearance is 500 mm. The required minimum rear clearance is 150 mm for correct air flow.