990-66239-001

Specifications

DANGER
hazard of electric shock, explosion, or arc flash
The modular battery cabinet must only be used with the Easy UPS 3S Pro.
Failure to follow these instructions will result in death or serious injury.
NOTICE
hazard of equipment damage
Refer to the UPS installation manual for detailed specifications for the UPS system.
Failure to follow these instructions can result in equipment damage.
Nominal battery voltage (V) Battery type Maximum number of battery strings Number of battery blocks per string Maximum short-circuit level (Icc)
480 Lead-acid 6 strings (24 battery modules) 40 Icc = 16 kA

Disconnect Device Battery Circuit Breaker Specifications

Type C16S4TM160D
Rating (A) 160
Withstand rating 100 kA
Ir 114 A (Easy UPS 3S Pro)
Im 1250 A