990-66239-001

Install Battery Modules in the Modular Battery Cabinet

  1. Remove the plate in front of the battery shelves.
  2. Holding the handle, install the battery modules one string at a time from the bottom and up.
    CAUTION
    Heavy load
    Battery modules are heavy and require two persons to lift.
    • The battery module weighs 27 kg.
    Failure to follow these instructions can result in injury or equipment damage.
  3. Push down the handle of each battery module and fasten it to the shelf with the provided screw in front of the battery module.

    Front View of Battery Module

  4. Remove the shrink tubes from the battery terminals and connect the battery terminals to the batteries.
  5. Reinstall the plate in front of the battery shelves.
For battery string configuration for different UPS rating, see Battery String Configuration for Easy UPS 3S Pro for details.