990-66239-001

Connect the Power Cables between the Easy UPS 3S Pro UPS and the Modular Battery Cabinet

NOTE: Route the signal cables separately from the power cables.
  1. Remove the packaging bag without cutting it – save the packaging bag for later use.

    Front View of the Modular Battery Cabinet

  2. Remove the conduit box from the rear of the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  3. Install the conduit box on the modular battery cabinet. Note that the conduit box is installed in the reverse position.

    Rear View of the Modular Battery Cabinet

  4. Remove the top cover from the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  5. Remove the installation kit from the top of the modular battery cabinet. The installation kit contains DC cables, hardware, and cable ties for interconnection between the modular battery cabinet and the UPS.
    • DC+ cable WH00141 (red)
    • DC N cable WH00142 (blue)
    • DC- cable WH00143 (white)
    • PE cable WH00146 (yellow and green)
  6. Cut holes on the cable brush plate on the conduit box.

    Rear View of the Modular Battery Cabinet

  7. Connect the supplied DC cables (DC+, DC-, DC N) to the UPS.
    1. Connect the provided PE cable and the DC cables (DC+, DC-, DC N) in the modular battery cabinet.
    2. Route the PE cable and DC cables (DC+, DC-, DC N) out through the conduit box and into the UPS power cabling area.
    3. Follow the UPS installation manual to connect the PE cable and DC cables (DC+, DC-, DC N) in the UPS.
      NOTE: The provided DC cables have an M6 connector on one end and an M8 connector on the other end. Select the appropriate connector size based on the UPS commercial reference. See DC Cable Connector Size Selection for details.

    Rear View of the Modular Battery Cabinet

    DC Cable Connector Size Selection

    UPS commercial reference DC cable end connector size - in the UPS DC cable end connector size - in the modular battery cabinet
    E3SP10KH, E3SP15KH
    E3SP20KH, E3SP30KH, E3SP40KH
    E3SP15KHIN, E3SP20KHIN
    E3SP30KHIN, E3SP40KHIN
    E3SP10K3I, E3SP15K3I
    E3SP20K3I, E3SP30K3I
    E3SP15K3IIN, E3SP20K3IIN
    E3SP30K3IIN
    E3SP10KHB, E3SP15KHB
    E3SP20KHB, E3SP30KHB
    E3SP10K3IB, E3SP15K3IB
    E3SP20K3IB
    M6 M8

    E3SP40KHB
    E3SP30K3IB

    M8 M6
  8. Fasten the power cables to the cable reliefs.

    Rear View of the Modular Battery Cabinet