Four E3SXR8 Units Connected in Parallel to Easy UPS 3S Pro UPS
- Connect battery cables between adjacent modular battery
cabinets.
-
DC+ of modular battery cabinet to DC+ of its adjacent modular battery cabinet
-
DC N of modular battery cabinet to DC N of its adjacent modular battery cabinet
-
DC- of modular battery cabinet to DC- of its adjacent modular battery cabinet
-
PE of modular battery cabinet to PE of its adjacent modular battery cabinet
-
- Connect the supplied battery cables (+, –, N) of modular battery cabinet 1 to the UPS as shown.
- Connect the signal cables between the modular battery cabinets.
Connect the signal cables for modular battery cabinet 1 to the UPS
as shown.NOTE: For Easy UPS 3S Pro for internal batteries, terminal J4-1 is occupied by the internal temperature sensor. Therefore, it is recommended to configure J3-5 as the battery temperature sensor, as this terminal is set as the ambient temperature sensor by default.
- Fasten the cables to the cable reliefs for all modular battery cabinets.
- Reinstall the top cover for all modular battery cabinets.