990-6408D-001

System Overview

Model List

All models may not be available in all regions.

  • E3SUPS10KFB: Easy UPS 3S 10 kVA 208 V 3:3 UPS for internal batteries

  • E3SUPS10KFBS: Easy UPS 3S 10 kVA 208 V 3:3 UPS for internal batteries, start-up 5x8

  • E3SUPS15KFB: Easy UPS 3S 15 kVA 208 V 3:3 UPS for internal batteries

  • E3SUPS15KFBS: Easy UPS 3S 15 kVA 208 V 3:3 UPS for internal batteries, start-up 5x8

  • E3SUPS20KFB: Easy UPS 3S 20 kVA 208 V 3:3 UPS for internal batteries

  • E3SUPS20KFBS: Easy UPS 3S 20 kVA 208 V 3:3 UPS for internal batteries, start-up 5x8

  • E3SUPS30KFB: Easy UPS 3S 30 kVA 208 V 3:3 UPS for internal batteries

  • E3SUPS30KFBS: Easy UPS 3S 30 kVA 208 V 3:3 UPS for internal batteries, start-up 5x8

  • E3SUPS40KFB: Easy UPS 3S 40 kVA 208 V 3:3 UPS for internal batteries

  • E3SUPS40KFBS: Easy UPS 3S 40 kVA 208 V 3:3 UPS for internal batteries, start-up 5x8

NOTE: Batteries are sold separately.

User Interface

Keys

Home Previous Next Confirm

EPO

Only use the EPO button in case of emergency.

It can be configured whether, when the EPO is activated, the UPS should:

  • turn off the rectifier, inverter, charger, and static bypass and stop supplying the load immediately (default), or

  • transfer to static bypass mode and continue supplying the load.

DANGER
hazard of electric shock, explosion, or arc flash
The UPS control circuit will remain active after the EPO has been pushed if utility/mains is available.
Failure to follow these instructions will result in death or serious injury.

Status LEDs

  LED Status
A Rectifier

Green : Rectifier is working correctly.

Flashing green : Rectifier is starting up.

Red : Rectifier is inoperable.

Flashing red : Utility/mains is unavailable.

OFF : Rectifier is off.

B Battery

Green : Battery is charging.

Flashing green : Battery is discharging.

Red : Battery is inoperable.

Flashing red : Battery low voltage.

OFF : Battery and battery charger are OK, battery is not charging or discharging.

C Bypass

Green : Load supplied by bypass source.

Red : Bypass source is unavailable or static bypass switch is inoperable.

Flashing red : Bypass voltage is out of tolerance.

OFF : Bypass source is OK.

D Inverter

Green : Load supplied by inverter.

Flashing green : Inverter on, start, synchronization or standby (ECO mode).

Red : Load not supplied by inverter, inverter is inoperable.

Flashing red : Load supplied by inverter, but an inverter alarm is present.

OFF : Inverter is off.

E Load

Green : UPS output is on.

Red : Overload on UPS output for too long, or output has shorted, or no output power present.

Flashing red : Overload on UPS output.

OFF : UPS output is off.

F Status

Green : UPS is OK.

Red : Inoperable status.

Display Interface

Home Screen

Buttons

Power On/Off Input and bypass status information Output status information Battery status information UPS status Function settings Log Mute

Overview of Single UPS

UIB Unit input breaker
SSIB Static switch input breaker
UOB Unit output breaker
MBB Maintenance bypass breaker
BB Battery relay

Overview of Parallel System

NOTE: In parallel systems with an external maintenance bypass breaker Ext. MBB, the maintenance bypass breakers MBB must be padlocked in the open position.
MIB Mains input breaker
BIB Bypass input breaker
UIB Unit input breaker
SSIB Static switch input breaker
UOB Unit output breaker
Ext. UOB External unit output breaker
MBB Maintenance bypass breaker
Ext. MBB External maintenance bypass breaker
SIB System isolation breaker
BB Battery relay

Location of Breakers

10 kVA UPS

15-20 kVA UPS

30 kVA UPS

40 kVA UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.