990-6426-001

Maintenance Bypass Panel Weights and Dimensions

  Weight kg (lbs) Height mm (in) Width mm (in) Depth mm (in)
E3SBPSU10K20F 30 (66) 600 (23.62) 550 (21.65) 260 (10.24)
E3SBPSU30K40F 65 (143) 900 (35.43) 800 (31.50) 320 (12.60)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?