990-6426-001

Connect the Power Cables

E3SBPSU10K20F

E3SBPSU30K40F

  1. Connect the ground cable.
  2. Perform one of the following:
    • For single mains: Connect the input cables to the unit input breaker (UIB).
    • For dual mains: Connect the bypass cables to the static switch input breaker (SSIB).
  3. Perform one of the following:
    • For single mains: Connect the UPS input cables to the unit input breaker (UIB).
    • For dual mains: Connect the UPS bypass cables to the static switch input breaker (SSIB).
  4. Connect the UPS output cables to the unit output breaker (UOB).
  5. Connect the load cables.
  6. Fasten the cables with cable ties to the cable reliefs as shown.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?