990-6426-001

Connect the Signal Cables

NOTE: Route the signal cables separately from the power cables.
  1. Remove the plastic cover of the maintenance bypass breaker MBB to get access to the auxiliary switch.
  2. Connect signal cables 22 AWG (not supplied) between the maintenance bypass breaker MBB and the UPS.
  3. Route the signal cables through the top or bottom of the maintenance bypass panel and fasten the signal cables to the cables reliefs.

    E3SBPSU10K20F – Top Cable Entry

    E3SBPSU30K40F – Top Cable Entry

    E3SBPSU10K20F – Bottom Cable Entry

    E3SBPSU30K40F – Bottom Cable Entry

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?