990-6426-001

Torque Specifications

Bolt size Torque
M6 on busbar 5 Nm (3.69 lb-ft / 44.3 lb-in)
M8 on busbar 17.5 Nm (12.91 lb-ft / 154.9 lb-in)
M10 on busbar 30 Nm (22 lb-ft / 194.7 lb-in)
5/32 in on breaker 9 Nm (6.64 lb-ft / 79.7 lb-in)
M10 on breaker 50 Nm (36.88 lb-ft/ 442.5 lb-in)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?