990-6426-001

Prepare the Maintenance Bypass Panel for Cables

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the parallel maintenance bypass panel.
Failure to follow these instructions will result in death or serious injury.
  1. Prepare the maintenance bypass panel for power and signal cables:
    1. Loosen the six bolts from the top AND bottom gland plates for power cables and remove the gland plates.
    2. Loosen the two bolts from the top OR bottom gland plate for signal cables and remove the gland plate.

    Top of Maintenance Bypass Panel

    Bottom of Maintenance Bypass Panel

  2. Drill or punch holes for cables/conduits.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Ensure that there are no sharp edges that can damage the cables.
    Failure to follow these instructions will result in death or serious injury.
  3. Install conduits (if applicable) and reinstall the gland plates.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?