DUG_SmartSwitch Push Wireless_WH-00

Editing a group

  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.
    The Device Control Screen appears.
  2. On the top-right screen, tap > Edit groups.
    TIP: Tap + Create a group to create a new group.
  3. Select the group and make any of the following changes:
    • Tap to change the group icon.

    • Tap to change the group name.

    • To remove a device, swipe left on the device and tap to delete it.

  4. Tap + Add lights / Add shutters to add a new device, or unselect the selected devices. Then tap Save to apply changes.
  5. On the Group Editor screen, tap Save to save the changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.