DUG_SmartSwitch Push Wireless_WH-00

Using the device

The Device Control Screen allows you to configure an Action/Moment/Group to the Wireless switch and control various settings.

On the Control tab, select the Wireless switch.

The Device Control Screen displays the following options:

A

Tap to configure an action, moment, or group (light/shutter) to the Wireless switch, such as turning on/off the lights, moving the shutter up or down, or any combination. For more information, refer to the following topics:

B

Tap to edit groups, such as adding or deleting devices, changing the group name, or icon.
You can also create a new group by tapping Edit groups > + Create a group. For more information, refer to Editing a group.

C

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

D

Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?