DUG_SmartSwitch Push Wireless_WH-00

Shutter Group

A shutter group is a group of shutter devices that are grouped together for a single control.

The shutter group can be assigned to the left or right push buttons. The shutter group requires two push buttons.

You can assign the same shutter group to multiple push-button pairs on a Wireless switch. For example, you can assign it to both pair 1 (left buttons) and pair 2 (right buttons). You can also assign the same group to multiple Wireless switch devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.