DUG_SmartSwitch Push Wireless_WH-00

Resetting the device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

When reset is done successfully. The Wireless switch and device returns to factory default.

  • Integrating into Wiser System

    • If you wish to integrate the device into Wiser System, reset all the devices in Quick Home Connect and pair it with the Wiser Hub.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?