0100DB2330_Trans

Interoperability with Third-Party Systems

For interoperability with third-party systems, EcoStruxure Power Monitoring Expert and Power Operation support OPC* DA* client and server functionality.

OPC is a set of open standards for connectivity and interoperability of industrial automation and the enterprise system. OPC provides a bridge between Windows-based applications and process control hardware, thereby eliminating the need for proprietary or custom interfaces and drivers for the various data types and sources residing in the corporate information network.

Additionally, EcoStruxure Power Operation provides extended OPC AE* server and OPC UA* client functionality.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.