0100DB2330_Trans

Overview of Digital Applications

Below is a summary of all the applications available in this guide. To ease selection, they have been grouped according to their end user benefits.

Click on any application below to navigate to it:

DIGITAL APPLICATIONS FOR ELECTRICAL SAFETY

Continuous Thermal MonitoringArc Flash ProtectionInsulation MonitoringGuided Procedures Through Extended Reality

DIGITAL APPLICATIONS FOR POWER AVAILABILITY

Electrical Asset Life Cycle ManagementAsset PerformanceElectrical Distribution Monitoring and AlarmingCapacity ManagementBackup Power TestingPower Event AnalysisCircuit Breaker Settings MonitoringPower Quality Monitoring and CompliancePower Quality CorrectionPower Source and Load ControlAdvanced Protection and AutomationOperator Training SimulationSimulate Before OperateMicrogrid

DIGITAL APPLICATIONS FOR SUSTAINABILITY

Utility Bill VerificationCost AllocationEnergy MonitoringEnergy BenchmarkingEnergy PerformanceEnergy Modeling and VerificationPower Factor CorrectionEnergy Efficiency ComplianceGreenhouse Gas Reporting
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?