0100DB2330_Trans

EcoStruxure Power Value Proposition

  • EcoStruxure Power digitalizes and simplifies low and medium voltage electrical distribution systems. It provides essential data to aid the decisions that help protect people, safeguard assets, maximize operational efficiency and business continuity, and maintain regulatory compliance.

  • EcoStruxure Power is an open architecture and platform designed with the intention of making it easy to add, upgrade, and swap components. The world is full of electrical distribution systems in various stages of maturity, produced by a variety of manufacturers. Interoperability with EcoStruxure Power is essential to making these power distribution systems future ready. The added benefit of a holistic Schneider Electric system is the plug-and-play connectivity to achieve faster and lower risk integration and commissioning.

  • EcoStruxure Power architectures are cost-optimized to deploy, using only the right technology to deliver the desired business outcomes for our customers – no more, no less. However, customer needs or demands change over time.

  • The EcoStruxure Power system is scalable from light commercial and industrial buildings to critical facilities such as hospitals, data centers, or infrastructure such as airports, rail, and energy and chemicals. The scalability of EcoStruxure Power means it also grows and evolves with changing needs or demands through its modular architecture.

  • EcoStruxure Power architectures are fully flexible power distribution systems with the ability to adapt to dynamic and ever-changing conditions, such as balancing supply and demand by the hour or minute or adding and then scaling on-site renewable generation capabilities over time. Connecting IT and OT systems into a single, easy-to-manage IP network is at the heart of our digitalization story. With EcoStruxure Power, facility managers can use the data they collect to make real-time decisions to maximize business continuity and optimize operations.

  • EcoStruxure Power architectures enable remote and on-site consultancy to help maximize uptime, optimize maintenance costs, and improve operator efficiency while extending asset and system life expectancy.

EcoStruxure Power Landing Page
Learn more about EcoStruxure Power, Schneider Electric’s digital solution for electrical distribution to help improve electrical safety, power availability, sustainability, and cybersecurity. Get access to customer testimonials, useful resources, and more!
https://www.se.com/ww/en/work/campaign/innovation/power-distribution.jsp

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.