0100DB2330_Trans

EcoStruxure Communication Drivers

EcoStruxure Power supports two types of communication drivers:

  • Native drivers for Schneider Electric connected products, including drivers for legacy connected products allowing modernization of systems with a step-by-step approach based on the life cycle of the assets

  • Drivers for third-party connected products using open protocols, such as Modbus, DNP3, IEC61850, BACnet, and OPC can be easily created to capture real-time data using purpose-built productivity tools in EcoStruxure Power Monitoring Expert and Power Operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?