Mounting the product
Wall box adjustment: If applicable, adjust the threaded-screw ring in the wall box such that the outer edge of the threaded-screw ring aligns with the surface of the wall.
- Mount the wall-insert into the wall box, with a maximum
tightening torque of 0.33 Nm for the screws. NOTE: Optional fixing mode by claw kit. (WDE002395)
- Remove the protection cap that covers the contact pins
on the rear side of the product, before mounting it into the wall-insert.NOTE: Any damage to the contact pins; for example, bending, breaking, or deformation, will interfere with the functioning of the product.
NOTICE damage to the contact pins- Handle the product carefully to avoid any damage to the contact pins.
- Make sure that the contact pins do not get damaged while mounting the product into the wall-insert.
Failure to follow these instructions can result in equipment damage. - Mount the product into the wall-insert using screws.
- Remove the protective film covering the surface of the product.