MFR2580802

Product overview

The Double Socket Outlet with 15 W USB charging ports and screwless terminals (referred to as product) consists of:

  • Two socket outlets (maximum 16 A shared on both)

  • Two USB charging ports (Type A and Type C, maximum 15 W shared on both)

On connecting the product to the mains, the socket outlets and the USB ports are energized.

The USB ports charge devices such as mobile phones, tablets, MP3 players and laptops. Up to two devices can be charged simultaneously. The USB LEDs indicate the charging status of the connected device(s).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?