MFR2580802

Operating the product

A

Socket outlets

B

USB Type A

C

USB Type C

D

USB LED indicators

When a device is connected to the USB port(s) for charging, the USB LED indicators indicate the charging status.

LED indication Status

When the device is charging, the LED glows in orange color.

When the device is 100% charged, the LED is off.

NOTE: Sometimes the LED flickers when the device is 100% charged because the device is consuming some current.
 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.