990-91380H-012

Caractéristiques du couple de serrage

Taille de vis Couple
M6 5 Nm (3,69 lb-ft / 44,3 lb-in)
M8 17,5 Nm (12,91 lb-ft / 154,9 lb-in)
M10 30 Nm (22 lb-ft / 194,7 lb-in)
M12 50 Nm (36,87 lb-ft / 442,5 lb-in)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?